Technical FAQs

Ask a Question

What are the maximum number of nodes supported by RIO network

RIO is fundamentally a single-master network and the RIO processor is the master node. The RIO processor is located in the PLC at the head-end of the RIO network.
 
Depending on the type of PLC being used, the RIO processor can be implemented in hardware, as an option module that mounts beside the PLC or as a board built into the PLC.

 
Was this helpful?
What can we do to improve the information ?