Technical FAQs

Ask a Question

What are the different Programming Languages available for Premium, Atrium, M340 & Quantum range PLC.

The following Programming Languages are available for Premium, Atrium, M340 & Quantum range PLC.
 
  1. Ladder Logic (LD)
  2. Functional Block Diagram ( FBD )
  3. Structure Text (ST )
  4. Sequential Function Chart ( SFC )
  5. Instruction List ( IL)
Note: 
For Quantum safety PLC only Ladder Logic ( LD) & Functional Block Diagram ( FBD ) is available.
Was this helpful?
What can we do to improve the information ?