Technical FAQs

Ask a Question

How to restart the READ_VAR and WRITE_VAR Communication without rebooting the Processor.

After the READ_VAR and WRITE_VAR communication halts there will be a need to reboot the Processor if the setting of the parameter ‘Communications timeout’ is left zero (Default value). 

A timeout value of zero will cause the function block to never timeout. 

This results in the READ_VAR and WRITE_VAR block to never close the TCP/IP connection when the Ethernet cable is disconnected and re-connected. The Processor will need to be stopped and re-started after the 
Ethernet TCP/IP cable is re-connected.
To resolve the issue, define a timeout value in the READ_VAR or WRITE_VAR block.
The timeout value time base is 100ms. Therefore if you enter 10 it will be 1 second.
Was this helpful?
What can we do to improve the information ?