Technical FAQs

Ask a Question

Is it possible that you can EXTEND the Premium CPU Sync Link using fiber cable and fiber Switches.

The use of an optical link with two switches for EXTENDING the Premium CPU Sync Link is forbidden today. Only an electrical copper link with a maximum 100 meter crossed cable can be used to EXTEND the Premium CPU Sync Link.
Was this helpful?
What can we do to improve the information ?