Technical FAQs

Ask a Question

What are the various stop error codes in Quantum HSBY

Stopcode 8xxx only means that the Quantum Processor is in Stop mode. The other various error codes that give more detailed information are tabulated below.

Machine Stop Code Descriptions:

Sr. No. Stop Bit Code (hex) Description
1 0x7FFF PLC Unhealthy
2 0x8000 PLC Stopped
3 0x4000 Bad I/O Traffic cop
4 0x2000 PLC in Dim awareness
5 0x1000 Bad port intervention
6 0x0100 Software error, controller in halt
7 0x0080 Watchdog timer has expired
8 0x0010 RIO option error
9 0x0001 Bad Configuration
Was this helpful?
What can we do to improve the information ?