Technical FAQs

Ask a Question

What are the features of new Quantum HSBY processor 140CPU67261 available in Unity Pro 5.0

Unity Pro V5.0 can be used to program the new Quantum HSBY processor (140CPU67261), which is designed primarily for infrastructure applications (tunnels, airports, railways and subways) with two main features:

1.) Extended Optical Fiber up to 10 km.

2.) Better Customer  Application performance, through an increased memory size (application size and execution time):
           a.) Internal SRAMs increased from 2 MB to 4 MB
           b.) L2 Cache Memory increased from 4 MB to 8 MB.
Was this helpful?
What can we do to improve the information ?