Technical FAQs

Ask a Question

How to resolve the problem of program retention for Quantum Processor on power recycle

The problem of program not retaining in the Quantum Processor on power recycle even when the battery is healthy is mainly due to the user application program corruption.

The most probable reason for the user application program getting corrupted is due to online changes and not proper build.

In order to fix this problem upload from the Processor the latest application program and transfer the application to *.XEF, restore it back, rebuild the program and download it to the controller.
Was this helpful?
What can we do to improve the information ?