Technical FAQs

Ask a Question

Which version of Web Designer software is compatible with M340 NOE Module (Ethernet) Firmware version 4.5 and 4.6

The Web Designer V2.22 is compatible with the M340 NOE Module (Ethernet) Firmware version 4.5 and 4.6 and should be used for designing the webpages.
Was this helpful?
What can we do to improve the information ?