Technical FAQs

Ask a Question

After downloading project to W@de it is not possible to access via Internet Explorer

The most probable reason for the W@de not been able to be accessed via Internet Explorer after downloading project could be due to the http port number to be configured differently.

By default the http port number is 80 on the W@de and for Internet Explorer.
If the http port number is changed in the configuration, Example: 1081 then the new command in Internet Explorer will be, if the IP address of the W@de is
Was this helpful?
What can we do to improve the information ?