Technical FAQs

Ask a Question

What is the maximum switching cycle of power permitted for Altivar71

The maximum number of times the power of the Altivar71 that is permitted to be switched is 1 cycle every minute. If the switching cycle is more in a minute the drive filter capacitors get stressed too much.

It is better to command the on/off of the drive by Logic Input.
Was this helpful?
What can we do to improve the information ?