Technical FAQs

Ask a Question

What is the procedure to save the program in Controller Inside optional card of Altivar 71 Drive

The "Controller Inside" card has a block of four programmable switches for configuration (see attached file.)

These switches can only be set when the drive and the "Controller Inside" card are turned off. Since it is necessary to remove the drive Control Front Panel in order to access it.

To save the program in the Controller Inside option card of Altivar 71 drive, first set the switch 4 = ON and then run the "Create Boot Project" in CoDeSys.

The program gets written in the flash memory. This process takes a few seconds.
The right-hand switch (switch 4) is used to protect the PS 1131 program in the Flash memory. The three left-hand switches can be programmed / set depending on the application.
Was this helpful?
What can we do to improve the information ?