Technical FAQs

Ask a Question

Which is the CANOpen address of the register that stores the Encoder Pulse Counts for Altivar 71 drive

The CANOpen address of the register is 201A/5 from where the Encoder Pulse Counts for Altivar 71 drive can be retrieved.
Was this helpful?
What can we do to improve the information ?