Technical FAQs

Ask a Question

Is Current Limit function available in Altivar 21 Drive

The Current Limit function is available in Altivar 21 Drive. The parameter number is F601.

The Current Limit range is 10-110% of drive's rated current. Factory setting is 110%.
Was this helpful?
What can we do to improve the information ?