Technical FAQs

Ask a Question

What is the accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 Drive

The accuracy of the displayed motor current on the Graphic Keypad of the Altivar 21 drive is approximately +/-10%.
Was this helpful?
What can we do to improve the information ?