Technical FAQs

Ask a Question

What is the accuracy of the Drive Power Consumption parameter APH in Altivar 71

The APH parameter allows to know the Altivar 71 Drive power consumption with a basic accuracy of 1Wh. 

The displayed value depends on total power consumption and can be in KWh or MWh but the calculation is always really with an accuracy of 1Wh maximum.
Was this helpful?
What can we do to improve the information ?