Technical FAQs

Ask a Question

What is the voltage drop with a AC Line Choke and with DC Choke in Altivar 71

The voltage drop with AC Line Choke is about 3% & 5%.
And with DC Choke the voltage drop is about 4% to 6% of the nominal supply voltage.
Was this helpful?
What can we do to improve the information ?