Technical FAQs

Ask a Question

How to reset the Altivar 71 Drive fault when in Terminal Control Mode

Logical Input assignment Menu --> Fault Management --> Fault Reset, one can reset the faulted Altivar 71 Drive from the Terminal when in Terminal Control Mode.

For Example LI3: 
When the Logic input LI3 is set to 1, Fault Reset happens.

Note:
In the Terminal Control Mode the reset button on the Graphic Keypad of the Drive is inactive.
Was this helpful?
What can we do to improve the information ?