Technical FAQs

Ask a Question

What is the ambient temperature of operation of Altistart 48

The nominal ambient temperature at which the Altistart 48 Soft Starter can operate is between -10oC to +40oC. 

Between + 40oC to + 60oC, the Altistart 48 can still be operated by derating it on the nominal current rating by 2 % for each °C.
Was this helpful?
What can we do to improve the information ?