Technical FAQs

Ask a Question

What does form Y203 mean on the 9007C series limit switches?

Issue:
What does form Y203 mean on the 9007C series limit switches?

Product Line:
IDSEN - sensors

Environment:
9007C

Cause:
product feature

Resolution:
The Form Y203 or (Y20-3) is for the factory modification to rotate the Turret head 180 degrees from its standard position.
However, this form is no longer available but the modification can be done in the field. The head can actually be rotated
 360 degrees in 90 degree increments.


CTA-ID : 12075
 
Was this helpful?
What can we do to improve the information ?