• Default Alternative Text

    Occupancy sensors

    Occupancy sensors make hands-free control of lights a reality.

  • zecelo main image ZENcelo Inspired by the fully-flat design trend that has transformed everything from airplane seats Inspired by the fully-flat design trend that has transformed everything from airplane seats and TVs to mobile phones and electric stoves, ZENcelo mechanical switches are ideal for interior design concepts that call for switches to be as unobtrusive as possible.
  • argus main image Argus ARGUS occupancy sensors automate the switching or dimming of lights by detecting movement within a space. They bring you convenient and the easiest way to eliminate lighting-related electricity wastage in unoccupied areas of your home or office. They even automates motor load switching for A/C, fans, blinds and curtains. Passive Infrared (PIR), Dual-tech (PRI+Ultrasonic) and dimmable sensors are available for various applications. Passive Infrared (PIR) occupancy sensors detect motion by sensing temperature profile changes, which is suitable for detecting large body movements.
  • neo main image NEO Based on art deco and tech-chic, NEO is a breakthrough in switch design. It demonstrates horizontal thinking, with unconventional horizontal dollies and layered details, and is the first mechanical switch to use LED locators and indicators. This is the forward thinking switch for forward thinking people.

Today's picks