• Default Alternative Text

    Telecommunication Accessories

    Getting connected is part of our daily lives.

  • ulti main image ULTI ULTI is for those who seek the haute couture in space design. With its ultra-clean lines, sleekly chic square profile and instantly identifiable round dollies, ULTI blends two contrasting geometries to create a modern simplicity of unprecedented freshness. The design also offers the maximum scope to showcase the synergy of colour, material and finish in a standard-sized wall plate.
    • ulti main image
    • Default Alternative Text
    • Default Alternative Text
  • neo main image NEO Based on art deco and tech-chic, NEO is a breakthrough in switch design. It demonstrates horizontal thinking, with unconventional horizontal dollies and layered details, and is the first mechanical switch to use LED locators and indicators. This is the forward thinking switch for forward thinking people.
    • neo main image
    • neo grey silver tel
    • Default Alternative Text
  • zencelo main image ZENcelo Inspired by the fully-flat design trend that has transformed everything from airplane seats Inspired by the fully-flat design trend that has transformed everything from airplane seats and TVs to mobile phones and electric stoves, ZENcelo mechanical switches are ideal for interior design concepts that call for switches to be as unobtrusive as possible.
    • zencelo main image
    • zencelo silver bronze telco
    • zencelo silver bronze telco data

Today's picks