• Default Alternative Text

    Wiser Home Control

    A centralized system that brings you comfort and convenience

    • DLT wallpates ulti 4gang DLT Wallplates
      Schneider Electric’s DLT Wall Switches feature “Dynamic Labeling Technology”, providing labels that show what each button does. What’s more they change automatically to indicate the status of 
      whatever they are controlling, such as different radio stations, light levels, even if your alarm is 
      armed or not. A Wiser home is an easy home!
    • 奥智 Zigbee 5场景手持遥控器 Scene Control Systems Scene control systems are used to control different light sources simultaneously, allowing different combinations of light sources to be switched on or off to the pre-set brightness. You can recall your pre-set scenes at one-touch of a button with wireless control available. There are two types of scene control systems: the 2-wire TruRetrofit that directly replaces the existing 2-wire mechanical switches, offering scene control without the hassle of rewiring; and the interoperable control system that suit situations where the whole house rewiring is done, providing more scene options and compatible with upgrades to home control system.