• Default Alternative Text

    Insights on the connected enterprise

Facilitating project execution in the connected enterprise

152831232-410x230

How the new generation of IIoT-ready controllers shorten time-to-value

Operational agility has always been important, but in an environment in which new connectivity pathways are emerging every day, it will be all but essential for survival. In addition to streamlining production operations, modern controllers contribute by enabling the localized control capability that enables faster response to changing market requirements and pressures.

By shortening the time it takes to adapt processes, they can help users take advantage of new business opportunities, expand operations, and even implement automation on greenfield projects.


…comprehensive libraries of preprogrammed software for many
common applications can greatly speed project time and substantially
cut costs..

To be truly of service, and help today’s application designer take full advantage of the opportunities awaiting within the IIoT, a controller should have at least the following characteristics:

• The power and bandwidth to handling increasingly complex production and
analytical calculations and higher speeds

• The Ethernet connectivity necessary to integration of production data with
operational, financial, supply chain and other enterprise data

• The built-in cybersecurity protection necessary to enable the benefits of open
integration with less risk of cyber protection

M580_IMG045-392x351

The Modicon M580 Ethernet-enabled
programmable automation controller (ePAC)
platform from Schneider Electric possesses
industry-leading processing and memory,
as well as stronger embedded cybersecurity. 

Project engineers using such modern, IIoT ready controllers within open programming environments can integrate them with the rest of the enterprise via open backplane and the Ethernet connectivity, In this way, instead of deploying a team of programmers to write custom code for each new installation or processing line, these modern engineering environments offer comprehensive libraries of preprogrammed software for many common applications. This can greatly speed project time and substantially cut costs.

To help companies take full advantage of these opportunities, systems integrators around the globe are gearing up to apply modern IIoT ready-controllers and advanced engineering environments. Also, automation vendors such as Schneider Electric have expertise in applying their technologies in numerous industries to gain competitive advantage by integrating new and legacy technologies to get new projects (brownfield) modernization or greenfield) up, running, and making money much sooner

For example, using IIoT-ready controllers can reduce time to market by 25% cutting up to three weeks from a typical three-month automation project. Assuming 120 production hours, at US$20,000 per hour, a plant can typically save more than US$2 million of extra production at launch.

And best of all, once deployed, these installations will be easier to modify, easier to scale, easier to maintain, and protected from cyber intrusion


For related information, click on any of the links below:

[White paper series] Preparing for the IIoT,  exploring the impact
M580 ePAC, the IIoT ready, Ethernet enabled Programmable Automation Controller
Improving productivity in the connected enterprise - How the new generation of IIoT-ready controllers connects you to new levels of operational efficiency
Energy management in the connected enterprise- How a new generation of IIoT-ready controllers improves energy efficiency
Seeing the Connections - How the new generation of IIoT-ready controllers reveals value hidden in process data

New value finder tool helps you discover $$ value hidden in plant assets
Try it now