• Default Alternative Text

    MOTION SENSORS

Motion Sensors

With all the increasing environmental concerns, everybody needs to save energy. Lighting is a good place to start with as it accounts for 20% to 30% of electricity consumption at home. So what should you sacrifice to save energy in lighting? Live in a darker home? No – simply install occupancy sensors, because the easiest way to save energy is to stop wasting it. People often forget to turn the lights off. Occupancy sensors help to eliminate lighting-related electricity wastage in unoccupied areas. It’s time to enjoy all the comforts and the lifestyle that electricity provides while still reducing energy consumption and doing your bit for the planet.