• Default Alternative Text

    Smart Water

    Smart Water

    Fresh water needs will grow by 20% in mature economies and by 50% in new economies by 2025. As populations grow and cities expand, it is essential to prevent flooding and provide clean and affordable water for consumption. Cities are where water is not always available but where people need it. Cities need to make their water smarter: more efficient, safe and available.

    We deliver smart water – today.
    Water distribution needs to be optimized, operational and energy costs reduced, and the whole water cycle made much faster than before. We help water agencies and utilities achieve up to 30% energy savings and up to 15% reduction of water losses through network and loss management systems, leak detection, energy and process optimization, stormwater management and urban flooding solutions.

    As cities grow, it is essential to provide clean and affordable water for consumption, as well as industries and irrigation. This means that water distribution needs to be optimized, operational and energy costs reduced. This is why water agencies and utilities worldwide are relying on Schneider Electric’s integrated solutions for optimal water and wastewater operations and planning. Similar to Smart Grid deployments in the energy industry, our advanced technology solutions support network operations efficiency and best practices. Components are highly integrated, assuring that data is complete, accurate, and secure, and that related operations are timely.