• Default Alternative Text
    Optimize end-to-end value chain and asset performance by integrating systems and processes

    Value Chain Efficiency

    Concrete Mixer truck

    Full chain visibility

    Cement producers lack visibility throughout the value chain with which to make effective decisions due to poor or missing data, siloed information, and minimal integration between systems.
    Looking up at construction

    Our Solution for Value Chain Efficiency

    Why work with Schneider Electric?

    • Default Alternative Text The market leader in cement energy management solutions As energy and cement experts, we understand how critical the efficient use of energy is in the production process.
    • Default Alternative Text Advanced solutions for plant performance and supply chain optimization Decision-support solutions for business, operational forecasting, planning and scheduling.

    Facts

    • Default Alternative Text It is estimated that there will be 30 billion connected "things" by 2020.
    • Blue ruler icon Given the bulky nature of the product and the associated high freight costs, transporting cement over 250 km (155 miles) is typically not economically viable.
    • Blue Graph up icon In India, the transportation cost of cement has gone up by 40% in just the last 2.5 years.
    • Blue lightning icon Cement consumption is seasonal and sensitive to external factors such as weather, bringing additional complexity to supply chain management.