• Solar panel farm in a flat and dry grassy plain, solar power, solar thermal panels, renewable energy
    RENEWABLE ENERGY

    RENEWABLE ENERGY

    Engineer with digital tablet standing in front of solar panels, energy management.

    Renewable energy alternatives

    Cement is an energy- and carbon fuel-intensive industry. As yields-per-ton continue to decline, and more raw material needs to be moved per unit of product, energy has become a significant cost factor. 

    • Solutions

      Technology and solutions needed to fully optimize energy usage through energy efficiency, energy management, renewable energy, and new energy technologies

      Our hybrid generation photo-voltaic systems, creating a hybrid system architecture that addresses the most economical energy mix.

    • Value Proposition

      In high irradiation areas, a low cost of energy (LCOE) can be achieved by Solar PV, making it affordable:

      • Solar PV is scalable, as plants are designed based on standardized building blocks.
      • Solar power systems can be built quickly, even in difficult climates.
      • Power can be produced where it is needed, and without transmission line losses.
      • Solar can be combined with diesel gen-sets and battery systems to form a micro-grid that does not rely on the primary grid.
    • Differentiation

      Schneider Electric has expertise in the key disciplines to deliver effective renewable-based systems:

      • Worldwide solution capabilities
      • Cement process experience
      • Solar power solutions
      • Micro-grid expertise
      • Integration of renewable energy into other systems

    Benefits

    • Cement factory at night, cement production.
      Reduced energy costs
    • Seaside industrial site, mining industry.
      Reduced impact on the environment
    • Cement facility at dusk, cement production.
      Greener and more sustainable operations