• Man inspecting metal coils, mineral processing


    Aluminium rolls in a warehouse, industrial production, mineral processing

    Mastering crane operations

    It is critical to track each coil of steel throughout every phase in the manufacturing process. Because each one represents a unique recipe — no two are exactly the same -- it is essential to intelligently track them, and the materials that comprise them.
    • Solutions

      Smart Crane Control:
      • Tracking and storage management.
      • Fast, efficient crane operation (sway / skew problems).
      • Material traceability and inventory visibility.
    • Value Proposition

      When used with warehouse management and positioning software, our sophisticated crane control solution tracks the position and location of each unit of steel, ensuring full traceability.


    • Engineers in steel forge control room, industrial automation, safety products
      • Higher productivity
      • Precise coil tracking and positioning
      • Less equipment stress
    • Steel worker working at an open electric steel furnace in an industrial foundry, industrial automation, mineral processing
      • Maximized system reliability and availability
      • Improved safety
    • Blast furnace pouring molten steel, mineral processing, manufacturing execution system
      • Reduced operation, maintenance, and repair costs
      • Extended equipment life