• Default Alternative Text

    Large Enterprise Building Management

    Energy and operational efficiency solutions

  • The Edge, Amsterdam SmartStruxure in the world’s most sustainable building

    The Edge sets a global benchmark for the sustainable building environment while prioritizing the comfort and well-being of occupants. Watch how SmartStruxure™ helps create an environment that is efficient and inspiring.

  • Davis School District, Utah, US

    Public school district, with 90+ buildings covering nearly 10M ft2, transitions from legacy building management system to SmartStruxure™ solution in three hours. Results: increased operation and energy efficiency and a productive learning environment.

  • Sheraton on the Park, Sydney, Australia

    Luxury hotel improves energy efficiency with upgrade to SmartStruxure solution building management system and saves 15% in energy costs, enabling it to take advantage of AusIndustry’s Green Building Fund.

    Read Story
    Default Alternative Text
  • GwangHwaMun D-Tower, Seoul, Korea

    SmartStruxure solution delivers energy management and occupant comfort at ultra-modern, mixed use twin towers (commercial office and retail building) in the "heart of Korea."

    Read Story
    Default Alternative Text
    Multi ethnic business people discussing work, energy efficiency, oil and gas

    Challenges

    Facing growing challenges, large enterprise building managers need a system to optimize energy consumption, maintain healthy and productive environments, and update aging facilities with anytime, anywhere access to information.
    Two men reviewing data on the computer screen, energy managment

    Our enterprise control systems

    From a single building to enterprise facilities.

    Customer Value

    • Integration icon Optimize building performance Gain significant financial savings during installation, operation and maintenance of your facility.
    • Handshake icon Maintain facility comfort and increase facility value Create a healthy, sustainable environment that increases occupant productivity.

    Facts

    • Blue Energy icon 40% of the world’s energy is used in buildings.
    • Blue tools icon 75% of a building costs over its lifetime will go to maintenance and operating expenses.
    • Default Alternative Text Only 20% of facility managers use 80% of their BMS's available capabilities.
    • Blue EcoXpert icon 30% of energy used in buildings is wasted because of inefficient BMS.
    • Blue interactive icon By 2020, there will be 30 billion devices connected via the Internet of Things.
    • Default Alternative Text In developed economies, at least half of the buildings that will be in use in 2050 are already built.