• Default Alternative Text
    Select the most efficient safety chain solutions for your machine

    Enabling movement safety function

    Default Alternative Text

    Challenges

    The enabling movement function is used to initiate movement of a machine to ensure that the operator is not within a dangerous area of the machine during movement. Operations during machine set up, maintenance and machine adjustments in close proximity of the dangerous areas on/within the machine are also possible to be managed using this function.
    Default Alternative Text

    Enabling movement safety function

    Select the most efficient safety chain solutions for your machine.
    • Safety Controller / Two Hand Control Station / Contactor / Cat.4 PL e, SIL 3 / Stop Category 0

      A complete enabling movement safety chain solution.
      Find Out More