• Default Alternative Text
    Select the most efficient safety chain solutions for your machine

    Perimeter guarding safety function

    Default Alternative Text

    Challenges

    The perimeter guarding function is used to protect the area around machines. It can be used to stop the machine (stop category 0, 1 or 2) directly or create a safe working zone wherein machine movements will not pass specific speeds, torque or position that could harm an operator. The function is commonly used when operators require regular intervention in a machine area.
    Default Alternative Text

    Perimeter guarding safety function

    Select the most efficient safety chain solutions for your machine.
    • Safety Module / Safety Mat / Contactor / Cat.3 PL d, SIL 2 / Stop Category 0

      Find Out More
    • Embedded Safety Module / Light Curtain / Contactor / Cat.4 PL e, SIL 3 / Stop Category 0

      Find Out More
    • Embedded Safety Module / Light Curtain / Variable Speed Drive / Cat.3 PL d, SIL 2 / Stop Category 1

      Find Out More
    • Safety Module / Single Beam Light Curtains / Contactor / Cat.2 PL c, SIL 1 / Stop Category 0

      Find Out More