• Default Alternative Text
    Select the most efficient safety chain solutions for your machine

    Speed monitoring safety function

    Default Alternative Text

    Challenges

    The speed monitoring function is used to monitor machine motor velocity. This is used to ensure velocity is within the proper range, according to the machine's functional requirements and design principles, before opening various parts of the machine.
    plexiglass safety walls around machine

    Speed monitoring safety function

    Select the most efficient safety chain solutions for your machine.
    • Safety Module / Remanent Voltage Detection and Limit Switch and Guard Switch with Lock / Contactor / Cat.4 PL e, SIL 3 / Stop Category 0

      Solution for speed monitoring
      Find Out More