Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Products and Services

            News

            Advanced Panel Magelis XBT GH, the perfect association of operability and safety

                  

            A handy panel to enhance mobility

            Regardless the industry applications, the portable Magelis XBT GH, allows operators to securely control and maintain their process from the best postion around the machine.
            Powered by Vijeo Designer, the single configuration software for Schneider Electric's HMI range, this mobile terminal is based on the same technology than other Advanced Panels : 

            • Touch screen 5.7"
            • VGA screen 65K colors
            • 11 Function keys with insert labels
            • Multiple communication interfaces with Serial line, Ethernet, USB and CF slot.

            Build rugged for tough conditions, this terminal offers a drop resistance conform to IEC 1131-2 with a IP65 body against moisture and oil.
            Schneider Electric paid a special attention for Safety :

            • Key switch to secure the use at start-up
            • Built-in emergency push-button (IEC60947-5-1)
            • 3-positions enable switch (dead-man switch)