Original Equipment Manufacturers
  1. VerticalNavigation :

    The navigation will be updated automatically.

 
 
 

Success stories - Simple machines

 
 

Vehicle manufacturer (Finland)

  Our customer, a Finnish vehicle manufacturer, operates in extreme climatic, corrosive and mechanical conditions. The firm decided to develop a robust unit capable of being mounted directly on the machine frame.

 

Benefits
- Exceptional resistance to severe environments (down to -20°)
- Simplified installation due to an enclosure-free mounting
- Significantly improved communication performance
- User-friendly interface featuring data management and video streaming

Main customer requirements
- Extreme temperature resistance of devices
- Resistance to regular vehicle high-pressure cleaning
- Shock and vibration resistance
- Touch-screen and joystick interfaces
- Reduced installation time

    

Our answer
Specially designed for use in severe conditions, our solution comprises the following components:
- Twido Extreme programmable controller
- Interfacing capabilities (Modbus, CANopen and CANJ1939 integrated in Twido Extreme)
- Advantys FTB and Magelis XBT GT