Schneider Electric India Frequently Asked Questions List (FAQs)



FA12166 : What is the Over-Voltage fault threshold of Altivar 31 Drive.

What is the Over-Voltage fault threshold of Altivar 31 Drive.


FA12208 : What is the maximum DC voltage per pole for TeSys F Range contactors.

What is the maximum DC voltage per pole for TeSys F Range contactors.


FA11563 : How to switch panels based on time in Magelis XBT G/GT terminals automatically.

How to switch panels based on time in Magelis XBT G/GT terminals automatically.


FA12101 : What are the minimum and maximum cable sizes recommended for use with TeSys D Star-Delta connection kits.

What are the minimum and maximum cable sizes recommended for use with TeSys D Star-Delta connection kits.


FA12178 : What is the maximum cable length allowed between PC and TeSys T for connection via PowerSuite.

What is the maximum cable length allowed between PC and TeSys T for connection via PowerSuite.


FA12160 : What is the maximum cable length allowed for connection of the Remote display of the Altivar 71 Drive.

What is the maximum cable length allowed for connection of the Remote display of the Altivar 71 Drive.


FA12204 : What is the maximum frequency in which Multi9 Range Residual Current Devices (RCD) can be used.

What is the maximum frequency in which Multi9 Range Residual Current Devices (RCD) can be used.


FA12132 : What is the Earth Leakage current value for an Altivar 31 Drive.

What is the Earth Leakage current value for an Altivar 31 Drive.


FA12108 : What is the difference between Utilization categories A and B in circuit breaker classification.

What is the difference between Utilization categories A and B in circuit breaker classification.


FA12146 : Is the Automatic adaptation of deceleration ramp feature available in Altivar 61 drive.

Is the Automatic adaptation of deceleration ramp feature available in Altivar 61 drive.


FA12147 : What is the DC Bus Voltage Threshold at which the Brake IGBT operates in Altivar 71 Drive powered with 220VAC or 415VAC 3 Phase.

What is the DC Bus Voltage Threshold at which the Brake IGBT operates in Altivar 71 Drive powered with 220VAC or 415VAC 3 Phase.


FA12148 : What Error 7 Fault means in the Altivar 58 Drive.

What Error 7 Fault means in the Altivar 58 Drive.


FA12149 : How Altivar 61 Drive can be auto started after Power ON.

How Altivar 61 Drive can be auto started after Power ON.


FA12150 : What is the Boot-up Time of Altivar61/71 Drives on Power Up.

What is the Boot-up Time of Altivar61/71 Drives on Power Up.


FA12151 : What is the meaning of OC1 fault in Altivar 21 Drive.

What is the meaning of OC1 fault in Altivar 21 Drive.


FA12152 : What is the booting time of Altistart 48 soft starter.

What is the booting time of Altistart 48 soft starter.


FA12153 : Is it possible to upgrade the firmware of Altistart 48.

Is it possible to upgrade the firmware of Altistart 48.


FA12154 : When does the cooling fan of Altivar 71 Drive start.

When does the cooling fan of Altivar 71 Drive start.


FA12155 : How to change the languages and the default Telemecanique Logo on the Keypad display for Altivar 61/71 Drives.

How to change the languages and the default Telemecanique Logo on the Keypad display for Altivar 61/71 Drives.


FA12156 : When does the INF3 (Internal Serial Link) fault occur in Altivar 61/71 Drive.

When does the INF3 (Internal Serial Link) fault occur in Altivar 61/71 Drive.


FA12157 : Is the braking transistor inbuilt in Altivar 71 Drives.

Is the braking transistor inbuilt in Altivar 71 Drives.


FA12145 : Is the remote keypad option available for Altivar 21 Drive.

Is the remote keypad option available for Altivar 21 Drive.


FA12158 : Is it possible to have dual connections from the Altivar 31 Drive ModBus Port.

Is it possible to have dual connections from the Altivar 31 Drive ModBus Port.


FA12159 : What is Evacuation function in Altivar 71 Drive.

What is Evacuation function in Altivar 71 Drive.


FA12180 : How to change the display settings of energy units from MWh to kWh in ME Meter.

How to change the display settings of energy units from MWh to kWh in ME Meter.


FA12181 : Does the Energy Reading remain stored for ME range Energy Meters during power failure.

Does the Energy Reading remain stored for ME range Energy Meters during power failure.


FA12182 : What is the use of the Terminal Numbers 5 to 10 on UA Controller in an Automatic Source-changeover System.

What is the use of the Terminal Numbers 5 to 10 on UA Controller in an Automatic Source-changeover System.


FA12183 : What is the latest Feature and Reference Number of MA500 trip unit for Compact NS630 MCCB.

What is the latest Feature and Reference Number of MA500 trip unit for Compact NS630 MCCB.


FA12184 : Is it possible to install OF/SD/SDE Auxiliary Contact (29450) in Single Pole and Two Pole Compact NS MCCBs.

Is it possible to install OF/SD/SDE Auxiliary Contact (29450) in Single Pole and Two Pole Compact NS MCCBs.


FA12185 : How does the Earth Fault protection work in Micrologic 6.0 when Neutral CT is not connected.

How does the Earth Fault protection work in Micrologic 6.0 when Neutral CT is not connected.


FA12186 : Is it possible to do remote reset function with ASI module ASILUF05 of TeSys U.

Is it possible to do remote reset function with ASI module ASILUF05 of TeSys U.


FA12187 : Is it possible to give Start/Stop commands from PLC via Modbus Port on LUCM module of TeSys U.

Is it possible to give Start/Stop commands from PLC via Modbus Port on LUCM module of TeSys U.


FA12189 : What is the noise level of TeSys D contactors and how to reduce the Noise during opening and closing of contactors.

What is the noise level of TeSys D contactors and how to reduce the Noise during opening and closing of contactors.


FA12190 : Is it possible to use LTME DC Expansion module with LTMR AC module of TeSys T.

Is it possible to use LTME DC Expansion module with LTMR AC module of TeSys T.


FA12191 : Is it possible to connect the different control voltages at the input of LTMR module in TeSys T.

Is it possible to connect the different control voltages at the input of LTMR module in TeSys T.


FA12192 : Is it possible to control the motor from TeSys T via the PowerSuite software.

Is it possible to control the motor from TeSys T via the PowerSuite software.


FA12193 : What is the maximum current which can be measured by TeSys T.

What is the maximum current which can be measured by TeSys T.


FA12194 : What is the short circuit current rating for TeSys GV2G Bus Bar.

What is the short circuit current rating for TeSys GV2G Bus Bar.


FA12210 : What is the maximum DC voltage per pole for TeSys D range contactors.

What is the maximum DC voltage per pole for TeSys D range contactors.


FA12212 : Is it permissible to electrically reverse feed the TeSys range of MPCB.

Is it permissible to electrically reverse feed the TeSys range of MPCB.


FA12213 : Is it possible to use TeSys GV2 and TeSys GV3 Range MPCB in DC applications.

Is it possible to use TeSys GV2 and TeSys GV3 Range MPCB in DC applications.


FA12214 : What is the maximum length of the connector cable between the LTMR and LTME module in TeSys T Range.

What is the maximum length of the connector cable between the LTMR and LTME module in TeSys T Range.


FA12215 : Can TeSys T be used downstream of Altivar range Variable Speed Drive.

Can TeSys T be used downstream of Altivar range Variable Speed Drive.


FA12216 : What is the maximum number of sensors and resistance values which can be connected to the T1 and T2 terminals on TeSys T.

What is the maximum number of sensors and resistance values which can be connected to the T1 and T2 terminals on TeSys T.


FA12217 : Can TeSys range overload relays be used in DC application.

Can TeSys range overload relays be used in DC application.


FA12218 : What is the compatibility between old D2 Range & TeSys D Range contactor accessories.

What is the compatibility between old D2 Range & TeSys D Range contactor accessories.


FA12219 : How to mount the Rectifier DR5TE on TeSys F range of contactor.

How to mount the Rectifier DR5TE on TeSys F range of contactor.


FA12221 : What is the Resistance value used in the capacitive contactor LC1D*K range.

What is the Resistance value used in the capacitive contactor LC1D*K range.


FA12188 : What is the Short Circuit rating of LU2B starters in TeSys U as per UL508 TypeE specification.

What is the Short Circuit rating of LU2B starters in TeSys U as per UL508 TypeE specification.


FA12144 : How to connect external potentiometer in Altivar 31 drive.

How to connect external potentiometer in Altivar 31 drive.


FA12143 : What is the meaning of elapsed time and power on time in the fault history of Altivar 71 drive.

What is the meaning of elapsed time and power on time in the fault history of Altivar 71 drive.


FA12142 : What is the maximum Ohmic value of the Braking Resistor for the Altivar 71 Drive.

What is the maximum Ohmic value of the Braking Resistor for the Altivar 71 Drive.


FA12141 : What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.

What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.


FA12140 : Which are the environmental conditions in which the Hoist Resistor of Altivar 71 Drive be used.

Which are the environmental conditions in which the Hoist Resistor of Altivar 71 Drive be used.


FA12139 : What is the version for the PDA/Pocket PC Power Suite or cut down version of Power Suite.

What is the version for the PDA/Pocket PC Power Suite or cut down version of Power Suite.


FA12138 : What is part reference for the Modbus to DeviceNet Gateway for the Altistart 48 Soft Starter.

What is part reference for the Modbus to DeviceNet Gateway for the Altistart 48 Soft Starter.


FA12137 : What is the difference between Fire Mode (Function 52) and Force Mode (Function 53) in Altivar 21 Drive.

What is the difference between Fire Mode (Function 52) and Force Mode (Function 53) in Altivar 21 Drive.


FA12136 : Which are the latest GSD file revisions for ProfibusDP communication board of the Altivar 71 Drive.

Which are the latest GSD file revisions for ProfibusDP communication board of the Altivar 71 Drive.


FA12135 : What is the heat dissipation (power loss) of the Passive Filter used for the Altivar 71 Drive.

What is the heat dissipation (power loss) of the Passive Filter used for the Altivar 71 Drive.


FA12134 : What is the Short Circuit Current Rating for Altistart 48 Range of Soft Starters for 415 Volt (Q series) and 690 volt(Y series).

What is the Short Circuit Current Rating for Altistart 48 Range of Soft Starters for 415 Volt (Q series) and 690 volt(Y series).


FA12133 : What are the dimensions of the detachable Keypad (VW3A31101)of the Altivar 31 Drive.

What are the dimensions of the detachable Keypad (VW3A31101)of the Altivar 31 Drive.


FA12131 : Which power phases are controlled by Altistart 01 Soft-Starter.

Which power phases are controlled by Altistart 01 Soft-Starter.


FA12130 : What is the maximum motor cable length allowed between the Sinus Filter and Altivar 71 Drive.

What is the maximum motor cable length allowed between the Sinus Filter and Altivar 71 Drive.


FA12129 : What is the reason of Free Wheel Stop Status (nSt) in Altivar 31 Drive.

What is the reason of Free Wheel Stop Status (nSt) in Altivar 31 Drive.


FA12128 : When does the Drive Overheat Fault (OHF) occur in Altivar 71 Drives.

When does the Drive Overheat Fault (OHF) occur in Altivar 71 Drives.


FA12127 : What is the minimum time interval allowed between two consecutive peaks of 220% Torque (Tn) in Altivar 71 Drive.

What is the minimum time interval allowed between two consecutive peaks of 220% Torque (Tn) in Altivar 71 Drive.


FA12126 : What are the different Communication Networks on which the Altivar 61 Drive can be communicated.

What are the different Communication Networks on which the Altivar 61 Drive can be communicated.


FA12125 : What is the meaning of the Speed-range ratio in Altivar 61/71 Range Drives.

What is the meaning of the Speed-range ratio in Altivar 61/71 Range Drives.


FA12124 : What is the minimum rating of the Motor that can be used with the Altivar 31/61/71 Range of Drives.

What is the minimum rating of the Motor that can be used with the Altivar 31/61/71 Range of Drives.


FA12123 : What are the MTTF (Mean Time to Fail, in hours) values for Altivar 61/71 Drives.

What are the MTTF (Mean Time to Fail, in hours) values for Altivar 61/71 Drives.


FA12122 : What is the setup procedure to establish the communication of Altivar 21 Drive via ModBus RTU or ModBus Network.

What is the setup procedure to establish the communication of Altivar 21 Drive via ModBus RTU or ModBus Network.


FA12121 : Which are the Drives in Altivar 31 Standard Range that has in-built Fan Units.

Which are the Drives in Altivar 31 Standard Range that has in-built Fan Units.


FA12120 : Is it possible to use Altivar 71 Drive for control of the Synchronous Motor.

Is it possible to use Altivar 71 Drive for control of the Synchronous Motor.


FA12119 : What is the minimum recommended Ground to Input Phase insulation resistance for Altivar 71 Drive.

What is the minimum recommended Ground to Input Phase insulation resistance for Altivar 71 Drive.


FA12197 : What is the Cross-sectional area of the Bus Bar conductors in Canalis KSA range.

What is the Cross-sectional area of the Bus Bar conductors in Canalis KSA range.


FA12195 : What is the total power dissipation per pole in watts of Vario Switches at the specified Thermal Current Rating (Ith).

What is the total power dissipation per pole in watts of Vario Switches at the specified Thermal Current Rating (Ith).


FA12116 : How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range.

How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range.


FA12115 : How to enable the Navigation Panel option in ProWorx32.

How to enable the Navigation Panel option in ProWorx32.


FA12114 : How can we set the time and date in Modicon PL7 Premium CPU.

How can we set the time and date in Modicon PL7 Premium CPU.


FA12113 : What are the various parts included in the LA91217 Star Delta connection kit.

What are the various parts included in the LA91217 Star Delta connection kit.


Execution Time : 58 milliseconds