Water
          Water logo

          Pump & Fan Control (Industry/Infrastructure)

          Pains & drivers

          • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% control pump or fan applications.
          • Most pump and fan applications are driven by a SoftStarter DOL solution. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge.
          • The CEMEP association has carried out a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year.
           

          How can a customer manage energy more efficiently?

          • To save energy you must:
            - drive the motor with a frequency inverter instead of a contactor or Soft Start
            - remove the restriction device (valve or damper)
          • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
          • The result is huge savings compared to conventional solutions:
            - up to 50% for a Fan, return on investment for the drive is within one year
            - up to 30 % for a Pump, return on investment within 2 years
           

          Solutions or architectures used in the application

           
          Solutions or architectures used in the application
          A) Solution without Drive
          The motor turns at a fixed speed according to the network frequency and the number of poles.
          Example: 3600 Rpm for 60 Hz
          2-pole motor
          The only way to adjust the Flow is a restriction device (damper) which generates losses.







          B) Energy Saving Solution with Drive
          The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
          The Flow is directly proportional to the speed.
          The damper or valve are no longer required.







          C) Energy Consumption with and without Drive
          Example for Fan Application

          Outlet damper
          Variable speed drive
          50% of energy saving at 80% of the nominal flow


          Example for Pump Application

          Control valve
          Drive
          30% of energy saving at 80% of the nominal flow 

           
           
           
          Schneider Electric Solutions
          Schneider Electric SolutionsFlexibilityProductivityEnergy cost savingInnovation


          Altivar 61, Tesys U...

          n/an/an/an/a
           
           
           

          To know more 

          Requests for Products and Services information

          Contact your Customer Care Centre now!