Water solution: Modular solution for pumping and additional treatment
Value proposition
Main drivers:
For booster or complex pumping stations.
Solution in brief:
Modular solution to manage more than 4 pumps and additional functions such as chlorination or tank management .
Value proposition:
Based on Altivar 61 drives, this solution allows you to reduce energy consumption by 20% to 30% on pumps depending on their characteristics. Energy savings are easily estimated via ECO8 software
Differenciationfactors:
Flexible, this solution proposes high diagnostic capabilities thanks to Transparent Ready features and its connection to the Ethernet Network.