Water solution: Optimised pumping for swimming pool

Value proposition
Main drivers
Value proposition
At 80% of the flow, power consumption drops by 50% using a variable speed drive!
Up to 30% energy savings, optimising water flows for any application, filtration, cleaning, spa and heating...
Differentiation factors
Minimise the pump energy costs by operating at the lowest possible flow rate.
Place a variable speed drive Altivar 11 between the circuit breaker and the motor to achieve flow variation by electronically controlling the speed of the motor.
Architecture

Main characteristics
The Altivar 11 drive combines all the functions that your application requires: