This image can't be displayed
   
 

Save up to 50% of design & installation time

 

> Download our System user guide & Wiring diagrams now

 
   
   
 

Machine Control Solutions

 

> Home

 
   
 
 
 

Safety Chain Selector

Reduce cost and machine design time thanks to the help of our "Safety Chain Solutions"

 
 

Schneider Electric provides you the means to get started on your machine adaptation of the new functional standards by using our certified ‘Safety Chain Solutions': a safety application example, based in a combination of interoperating products to realize a safety function, that includes an approved principle diagram and the correspondent safety level calculation.

They allow you to save time and cost in obtaining the machine certificate according to the new European Machinery Directive by including it like a complementary documentation.

They can be easily selected, according to your safety level and application required, by means of our safety selector tool. 

We recommend that you contact our specialists who can advise you. 

Search in Progress...

Loading
  
 
To know more

To know more 

Contact us

contact your customer care center
 
 
 
 
 
 

(*) Determination of the Performance Level requested (PLr)

 

      This determination could be done using the risk graph (see figure).

     S = Severity of injury
     S1 = Slight (normally reversible injury)
     S2 = Serious (normally irreversible) injury including death

     F = Frequency and/or exposure time to the hazard
     F1 = Seldom to less often and/or the exposure time is short
     F2 = Frequent to continuous and/or the exposure time is long

     P = Possibility of avoiding the hazard or limiting the harm
     P1 = Possible under specific conditions
     P2 = Scarcely possible

     L = Low contribution to risk reduction
     H = High contribution to risk reduction

 

(**) Categories of safety stop

International standard EN/ISO 13850 specifies the functional requirements and design principles of emergency stop devices.

It applies to all machines, whatever type of energy is used to control this function.
    

The standard allows two types of stop:

  •  Category 0 : stopping by immediate cutting-off of power or mechanical disconnection between the dangerous components,
  • Category 1 stop: controlled stopping with power maintained to the actuator to achieve stopping (braking for example),
                then cut-off of power when standstill is reached.
        

 The choice between these two stopping methods is determined by an evaluation of the machine-related risks.