India|[Global Website]|Home|Site map|Contact
 Search form button

VerticalNavigation :

The navigation will be updated automatically.

   
 

Back to the water segment

 
   
 
 
 

Solution: Compact pumping solution for lifting stations, small pumping stations or reservoirs

 
 

 

 
 

Value proposition

 
Main drivers:
  • Dedicated to lifting, small pumping stations or tank stations with a maximum of 2 pumps to manage.

Solution in brief:
  • This implementation constitutes an optimised, compact solution that provides the most interesting process data, such as water level, flow and pressure.

Value proposition:
  • Manage a large network of pumping stations thanks to a telecommunication system reducing operating costs by 20%.

Differenciation factors:
  • Pre-configured application
  • Multiple standards: GSM, PSTN, Radio, leased line
  • Protocol availability: Modbus, IEC870, DNP3
  • Support of local team and partners by specialists
 

Solution architecture