FAQ Search

What is the Temperature Threshold at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled.

The Temperature Thresholds at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled are as follows: 

1. Start – Heatsink Temperature > 50°C. 
 
2. Stop – Heatsink Temperature < 40°C.
FA12172  |  12-Jul-2012  | Operating System
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful