FAQ Search

Is it possible to connect the different control voltages at the input of LTMR module in TeSys T.

Control Voltage characteristics 

You can connect different control voltages on the input of the LTMR TeSys T module, if the voltage and current ratings fall within the electrical specifications of the module. 
Also, you can connect an external power supply on the LTMR input if you connect the A2 of the product with the 0V AC/DC of the external power supply.
FA12191  |  21-Dec-2012
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful