FAQ Search

How many high speed Inputs/Outputs are available for Modicon M258 Controller.

All Modicon M258 controllers have two groups of high-speed Inputs/Outputs with, for each group:
Four sink type high-speed inputs(up to 200 KHz),2 standard inputs and 2 source type high-speed outputs (up to 100 KHz) dedicated 
to HSC( High Speed Counter) or PWM (Pulse Width Modulation) functions.
 
A high-speed input which can be used as an “Encoder capture input”
Two commons for the inputs.
One common for the outputs.
 
A power supply (24VDC) consisting of 3 units:
One for the CPU (Control Processing Unit).
One for the high-speed Input/Output modules.
One for other modules (Internal Input/Output Bus).
FA144856  |  21-Dec-2012  | Programming
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful