FAQ Search

Is it possible to use two Extended I/O Cards in one Altivar 71 drive.

It is not possible to use two I/O Extension cards in one Altivar 71 drive. However, it is possible to use one VW3A3201 Logic I/O
Card & one VW3A3202 Extended I/O Card in
one Altivar 71 drive.
Refer to attached file for Option Card compatibility.
 
FA145819  |  21-Dec-2012  | Hardware Compatibility
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful