What is the Input/Output (I/O)Capability for M218 Controller.
The Input/Output(I/O)Capability for Modicon M218 Controller is as follows:
1.M218 24 I/Os controller can be expanded with up to 4 expansion modules with operating limits of 152 I/O’s maximum,within 42
relays output maximum.
relays output maximum.
2.M218 40 I/Os controller can be expanded with up to 7 expansion modules with operating limits of 248 I/O’s maximum,within 90
relays output maximum.
relays output maximum.
Answers which others found helpful |