Is it possible to padlock the C60 MCB.
For padlocking the C60 MCB use part reference 26970. Find attached the Installation Manual for the same.
Note:
For 3P, 3P+N and 4P MCBs, use 2 numbers of 26970.
Attachment(s):
26970_Padlock_IM.pdf
(PDF,101K)
FA22611 |
12-Jul-2012
PDF
Email
Bookmark
Print
Answers which others found helpful
> If the C60H circuit breaker is locked ON with the MGLA padlocking facility will it still trip under fault conditions.
> What is the operating temperature range of the C60H circuit-breakers.
> Is it possible to install the C60 range MCB up side down.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel