What is the maximum angle at which CT Contactor can be mounted for normal operation.
The maximum angle at which CT Contactor can be mounted in relation to the normal vertical mounting plane from the rail is 45 degrees, for proper operation.
FA22616 |
13-Jul-2012
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the thermal class temperature for coil of CT Contactor.
> What is the Power dissipation for CT contactors according to different ratings.
> Is it possible to mount a surge suppressor with LED (LAD4RCE) on the CA4KN**, low consumption DC control relay.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel