Is it possible to connect Tm Remote Control 18311 with C120.
The Tm Remote Control, reference-18311 is designed only to use with C60 MCB not with the C120 MCB. Tm remote control, reference- 18312 is for C120 (2Pole).
It is not recommended to use the 18311 for C120 (2Pole) MCB as the inrush current for 18311(TmC60-4P) is lower than the 18312 (TmC120-2P).
Answers which others found helpful |