Can I connect aluminium or copper, flexible or rigid cables to the single and double terminals of the NSX 400 to 630 range.
In the NSX 400 to 630 range:
Single terminals, part numbers LV432479 or LV432480, can take: aluminium or copper rigid cables with cross-section 35 to 300 mm² and flexible cables with cross-section 240 mm² maximum.
Double terminals, part numbers LV432481 or LV432482, can take: aluminium or copper rigid cables with cross-section 35 to 240 mm² and flexible cables with cross-section 185 mm² maximum.
Single terminals, part numbers LV432479 or LV432480, can take: aluminium or copper rigid cables with cross-section 35 to 300 mm² and flexible cables with cross-section 240 mm² maximum.
Double terminals, part numbers LV432481 or LV432482, can take: aluminium or copper rigid cables with cross-section 35 to 240 mm² and flexible cables with cross-section 185 mm² maximum.
Attachment(s):
Answers which others found helpful |