{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I replace a broken toggle on an NS / NSX circuit-breaker or switch.?

No, the toggle on the breaker frame cannot be replaced as the toggle is integral to the breaker frame.

The breaker frame needs to be replaced.

However, the toggle extension (4 to 5 cm long piece screwed to the toggle) can be replaced, but only if the toggle thread is not damaged.

If the thread is damaged the breaker frame needs to be replaced.

For the NSX up to  250A - Part number is LV429313
For the NSX 400A to 630A - Part number is LV432553

Schneider Electric India

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.